Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What gauge of steel is used for NEMA 1, QO load center enclosures?
Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Gauge of Steel

Cause:
Application

Resolution:
The enclosures are manufactured from 16 gauge steel, except for the QO2L30F or QO2L30S, which is 18 gauge.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings