How do you short out a neutral CT for NT, NW, P or R breakers when it is installed, but you don`t want to use it? Do jumpers need to be added?
Issue:
Sometimes an installed circuit breaker is connected to an installed neutral CT, and there is a need to disconnect the NCT wires from the breaker, but the neutral CT cannot be physically removed from the equipment. When the NCT wires are disconnected, is there a need to add any jumpers to the NCT terminals?
Product Line:
Circuit Breakers
Environment:
Applies only to Masterpact NT, NW, and PowerPact P and R circuit breakers
Resolution:
For Masterpact NT, NW, or PowerPact P or R Circuit Breaker with neutral CT already installed, in order to disconnect the NCT from the breaker without removing the NCT from the equipment, follow these steps:
NEUTRAL CT'S WITH TERMINALS LABELED T1, T2, T3, T4
(1) De-energize the equipment
(2) NCT terminals
OLDER NEUTRAL CT'S WITH TERMINALS LABELED SG1, SG2, X1 and X2
(1) De-energize the equipment
(2) NCT terminals
Sometimes an installed circuit breaker is connected to an installed neutral CT, and there is a need to disconnect the NCT wires from the breaker, but the neutral CT cannot be physically removed from the equipment. When the NCT wires are disconnected, is there a need to add any jumpers to the NCT terminals?
Product Line:
Circuit Breakers
Environment:
Applies only to Masterpact NT, NW, and PowerPact P and R circuit breakers
Resolution:
For Masterpact NT, NW, or PowerPact P or R Circuit Breaker with neutral CT already installed, in order to disconnect the NCT from the breaker without removing the NCT from the equipment, follow these steps:
NEUTRAL CT'S WITH TERMINALS LABELED T1, T2, T3, T4
(1) De-energize the equipment
(2) NCT terminals
- Remove the wires from NCT terminals T1 and T2 (there is no need to jumper those terminals)
- Make sure there is a jumper between NCT terminals T3 and T4
- Remove the wires from breaker terminals T1 and T2, and ADD A JUMPER between breaker terminals T1 and T2
- Do NOT add add a jumper between breaker terminals T3 and T4
OLDER NEUTRAL CT'S WITH TERMINALS LABELED SG1, SG2, X1 and X2
(1) De-energize the equipment
(2) NCT terminals
- Remove the wires from NCT terminals SG2 and SG1 (there is no need to jumper those terminals)
- Make sure there is a jumper between NCT terminals X1 and X2
- Remove the wires from breaker terminals T1 and T2, and ADD A JUMPER between breaker terminals T1 and T2
- Do NOT add add a jumper between breaker terminals T3 and T4
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.