Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an adapter for connecting an old I-Line I busway to a new I-Line II busway?
Issue:
Old I-Line I busway to a new I-Line II busway connector part number

Product Line:
ILINE I Busway and ILINE II Busway

Environment:
Application using existing ILINE I Busway

Resolution:
Yes, you would add suffix 12S to I-Line II busway prefix if existing busway ends with a bolted end. You would add suffix 12B if existing busway ended with a slotted end. An example part number would be AF2516G12B.

busway

Note
  • The adapter will take 12 in. This should be consider when replacing existing busway.

See the Busway Systems Catalog https://www.se.com/us/en/download/document/5600CT9101 for more information.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings