Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What mechanical interlock attachment is used in the QO48M30DSGP and QO48M60DSGP, series G03 generator panels?
Issue:
Product Design

Product Line:
QO LC

Resolution:
The QO2DTI mechanical interlock is used. Two PK2MB retaining kits are also used to retain the backfed main breakers. Catalog number QO2DTIM would include the mechanical interlock and the two retaining kits in one kit.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings