Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can a SDSA1175 be installed into a load center?
Issue:
Installation of SPD into load centers.

Product Line:
Load centers and Surge Protection Devices

Environment:
SDSA, QO, HOM

Resolution:
The recommended installation of the SDSA1175 is to be connected to a 2-pole 20A branch circuit breaker (installed as close as possible to the main lugs or main breaker). The other way this device can be installed is by direct buss connecting it in a Square D QO or Homeline load centers using a QOSAMK mounting kit. This kit also includes hardware to connect the SDSA1175 leads to the load side of the main circuit breaker.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings