Issue:
Are auxiliary contacts available for the 8911 definite purpose starters?
Product Line:
Definate Purpose starters and contactors
Environment:
8910DPA and 8911DPS
Cause:
Additional accessories required for the application
Resolution:
Auxiliary contacts are available for the 8911DPS type devices, select from the chart listed below:
Maximum of two modules per contactor, one module per side:
This also applies to the 8910DPA contactors
The 8911DS compact units will not accept auxiliary contacts, other means of holding circuit must be supplied or maintained control contacts must be used.
Are auxiliary contacts available for the 8911 definite purpose starters?
Product Line:
Definate Purpose starters and contactors
Environment:
8910DPA and 8911DPS
Cause:
Additional accessories required for the application
Resolution:
Auxiliary contacts are available for the 8911DPS type devices, select from the chart listed below:
Maximum of two modules per contactor, one module per side:
| Contact arrangement | 20-90 amp series B and series C after date code 1401 | 20-40A series C before date code 1401 |
| 1 N.O. | 9999D10 | 9999DD10 |
| 1 N.C. | 9999D01 | 9999DD01 |
| 1 N.O./1 N.C. | 9999D11 | 9999DD11 |
| 2 N.O. | 9999D20 | 9999DD20 |
This also applies to the 8910DPA contactors
The 8911DS compact units will not accept auxiliary contacts, other means of holding circuit must be supplied or maintained control contacts must be used.
Released for: Schneider Electric Canada