Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the mounting pan used to install a subfeed Q2 or Powerpact Q-frame breaker in an NQOD panel?
Issue:
Installing subfeed Q2 or Powerpact Q-frame breaker in NQOD panelboard

Product line:
NQOD panelboards, Q2 and Powerpact Q-frame breakers

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Mounting pan required for a Q2 or Powerpact Q-frame subfeed breaker in an NQOD panelboard

Resolution:
NQOD panelboards were designed to accept KAL, KHL or Q2 frame circuit breakers. To install a Q2 or Powerpact Q-frame subfeed breaker, a mounting pan was required. This mounting pan elevates the breaker so that it meets the back of the deadfront properly. The mounting pan was part number 80110-054-01 (obsolete), now replaced by 80110-054-02. Quantity (4) mounting screws, part no. 21590-170-81, are also needed

Mounting pan is required when replacing a KAL/KHL subfeed breaker with a Q2 or Q-frame breaker in any NQOD panelboard, or when adding a second subfeed breaker to an existing 400A or larger NQOD panelboard.

Schneider Electric Canada

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings