Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is Form Y239 for the 8910/8911/8965 contactors?
Issue:
What is Form Y239 for the 8910/8911/8965 contactors?

Product Line:
Definite Purpose Contactors, Starters, and Hoist Contactors

Environment:
Products sold and used in the United States

Cause:
Identifying Options on Contactors

Resolution:
Substitute aluminum (40 amp) box lugs (as shown below) for standard terminal screws on line & load side (unless otherwise noted )of devices listed below.

Class 8910 Type DP 20 thru 40A (Standard on 40A)
Class 8910 Type DPA 20 thru 40A
Class 8910 Type SYD - Not valid on any Type SYD device
Class 8911 Type DPS 20 thru 40A - Line Side ONLY
Class 8911 Type DS 20 thru 30A - Line Side ONLY
Class 8965 Type DPR 20 thru 40A

List adder pricing and additional notes are as follows:
Class 8910 Type DP 20 thru 30A List Price Adder: $3.20 / Pole
Class 8910 Type DPA 20 thru 40A List Price Adder: $3.20 / Pole
Class 8911 Type DPS 20 thru 40A List Price Adder: $3.20 / Pole (Overload relay will have standard connectors)
Class 8911 Type DS 20 thru 30A List Price Adder: $3.20 / Pole (Overload relay will have std wire pressure connectors)
Class 8965 Type DPR 20 thru 40A List Price Adder: $6.40 / Pole (all units are considered 3 pole)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings