How can we help you today?

Can the user add power poles to the D Line contactors?

Issue:
Use of add power poles to the D Line contactors

Product Line:
Tesys D contactors

Environment:
IEC contactors

Resolution:
No. The D Line contactors are available with a maximum of 4 poles and no power pole modules exist.