How can we help you today?

Is the coil for the 8501 XO latching mechanism rated for continuous duty?

Issue:
Identify if the 8501XO Coil latching mechanism is rated for continuous duty.

Product Line:
Relays and Timers

Environment:
8501 Type X Relays​​​​​​​

Resolution:
Yes, the coil is continuous duty rated.