Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an LAD6K10*?
Issue:
Detail about LAD6K10*

Product Line:
Tesys D line Contactors and Accessories

Environment:
North American Products

Resolution:

It is a mechanical latch attachment for the LC1D09 through D38 TeSys D-line contactors. It can not be used on the pre-TeSys style contactors.
See below table for coil voltage codes to finish this part number:
Volts122432/3642/4860/72100110/127200/208220/240380/415440/480500/600
AC or DCJBCEENKFLMQRS

Note: The DC, low consumption contactors ( coil code *L) are not compatible with the mechanical latch blocks LAD6K10*.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings