Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What quantity and size of conductors can be used on a 400SN neutral assembly?
Issue:
Product feature

Product Line:
CB Enclosure

Resolution:
The 400SN accepts (1) #1 AWG - 600 kcmil or (2) #1/0 AWG - 250 kcmil aluminum or copper conductors, in and out. Two service grounding lugs each accept (1) #4 AWG - 300 kcmil aluminum or copper conductor.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings