Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a shunt trip accessory be provided on the Main Breaker of a QO or Homeline, Single Phase load center?
Issue:
Product Design feature

Product Line:
QO load centers

Environment:
Main breaker accessories

Cause:
Application

Resolution:
The Older Series 001, 002 or A02 Homeline main breaker load centers used a HOM2100, HOM2125, HOM2150 or HOM2200 main breaker. These main breakers do NOT have a shunt trip accessory available.
For the more recent or current series 'S' load centers that use a QOM1 Frame main breaker, a shunt trip accessory is NOT available.

For the more recent or current series 'S' load centers using the QOM2 Frame main breaker a shunt trip accessory is available factory installed ONLY. But it would require a Main Lug Load Center to be ordered and the QOM2 Main Breaker with the shunt trip accessory, suffix '1021', to be ordered separately and field installed. Also, a replacement QOM2 main breaker can be obtained with the shunt trip factory installed.

If ordering a replacement main breaker only, order the main breaker catalog number with the suffix '1021'. For example, QOM2200VH1021. See current digest for ALL QOM2 main breaker catalog numbers.

NOTE:
If a shunt trip is needed for the QOM1 Load center application, consider using a separate circuit breaker enclosure for a QO breaker with a shunt trip upstream of the load center.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings