Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there any restrictions regarding the installation mounting orientation of heavy duty, general duty, and double throw safety switches?
Issue:
Product Design

Product Line:
Heavy Duty, General Duty and Double Throw Safety Switches

Resolution:
Safety switches of all NEMA types are UL tested in an upright (vertical) position ONLY, with the 'ON' in the up position of the switch.

NOTE: There are no known objections to mounting a NEMA 1 switch on its side, BUT this is dependent upon interpretation of the local code authority. Consideration should always be given to allow full movement of the operating handle and front cover.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings