Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What factors affect the choice of a resistor/capacitor RC suppressor or a varistor suppressor?

Article available in these languages: Greek

Issue:
Why would an RC suppressor be used instead of a varistor?

Product Line:
Suppressors

Environment:
Schneider Electric Products

Resolution:
1) The RC units are used with AC coils only. The varistor units are used with AC or DC coils
2) The RC units drop out time is 1.2 to 2 times normal compared to the varistor 1.1 to 1.5 times normal.
3) The RC unit limits transient voltage to 300% of the nominal voltage maximum compared to a varistor 200% of nominal voltage maximum.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings