Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the Mini-Power Zones (MPZ) offered by SquareD/Schneider Electric marked per cUL, cULus, or CSA as suitable for use in Canada?
Issue:
Marking of Mini Power Zone Transformers

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone Transformers from SquareD/Schneider Electric

Cause:
Mini Power Zone Transformers are primarily designed and built for use in the USA

Resolution:
No, the MPZ product line is UL listed and labeled only. They are not CSA certified for Canada.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings