Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 9421NW2, NW2B, NW3, and NW3B operators rated for outdoor use?
Issue:
What NEMA rating do the 9421NW2, NW2B, NW3, and NW3B operators have?

Product Line:
Class 9421 Circuit Breaker Operating Mechanism

Environment:
Operating Mechanisms for Circuit Breakers

Resolution:
These handles are rated NEMA 1/12/4/4X and can be used with enclosures suitable for outdoor use.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings