Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does the overload relay on an 8536 type S starter work if the overload contact is normally open?
Product Line:

NEMA style Overload Relays

Resolution:
The normal position is with thermal units installed in all 3 poles and the pawl arms down. The thermal unit wheels hold the pawl arms down which, in turn, hold the overload contact closed. In an overload condition, 1 or more of the thermal unit alloy pots heats up and melts the alloy, allowing the wheel to move and release the pawl arm. This mechanically opens the contact and cuts control power to the coil. After cooling down, the alloy resolidifies and allows the overload to be reset.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings