Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Square D Heavy Duty Safety Switches UL Listed for use on photovoltaic (solar) applications?
Issue:
Product UL listing

Product Line:
Heavy Duty Safety Switches

Environment:
UL listing

Cause:
Application

Resolution:
Please refer to the Data Bulletin 3110DB0401R0410, Dated 6/2010, see attached below. The wiring diagrams shown on Page 1, Figures 1B, 1D or 1F can be used on a photovoltaic system and be within the UL listing of the switch. The wiring diagram shown on Page 2, Figure 2, can be used but is not within the UL listing of the switch. However, we have self-certified this method of wiring, for a photovoltaic system only, when applied per the limitations outlined in the Current Ratings table located below Figure 2.

Schneider Electric Canada

Attachment(s)
3110DB0401R0410 _June 2010.pdf [162.9 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings