Issue:
Identifying Part Number to field install start stop push buttons in a NEMA device
Product Line:
NEMA Contactors and Starters
Environment:
Products sold and used in the United States
Cause:
Field installing start stop push buttons
Resolution:
It is the 9999SA3 for NEMA 3R, 4 & 12 and the 9999SA13 for NEMA 4/4X stainless steel. User-made openings are required in order to field install these kits on standard 8536 NEMA Sizes 0 through 2 starters in NEMA 4 and 12 enclosures.
CTA-ID : 2007047
Identifying Part Number to field install start stop push buttons in a NEMA device
Product Line:
NEMA Contactors and Starters
Environment:
Products sold and used in the United States
Cause:
Field installing start stop push buttons
Resolution:
It is the 9999SA3 for NEMA 3R, 4 & 12 and the 9999SA13 for NEMA 4/4X stainless steel. User-made openings are required in order to field install these kits on standard 8536 NEMA Sizes 0 through 2 starters in NEMA 4 and 12 enclosures.
CTA-ID : 2007047
Released for: Schneider Electric Canada