Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a single phase pump panel?
Issue:
Is an 8940 Pump Panel Available for Use on Single Phase Loads?

Product Line:
NEMA Contactors and Starters

Environment:
Class 8940 Pump Panels

Resolution:
No, these devices are UL Listed as Service Entrance Equipment and have no single phase ratings or Listings.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings