Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are Mounting feet or channels available to floor-stand an I-line or QMB Panelboard (400A to 1200A)?
Issue:
Is there a way to make an I Line or QMB panelboard floor standing?

Product Line:
I Line and QMB Panelboards

Environment:
Application

Resolution:
Mounting feet, or Base Channels, are not available for NEMA 3R enclosures. However a "free standing" enclosure is available with welded base channels attached to back box.
This is a "Factory assembled Only" option.

See the attached file for more information.

feet

Schneider Electric Canada

Attachment(s)
Supplemental 177 Digest Panelboards D_0100CT1502_SEC-04.pdf [933.09 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings