Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the length of a 1091S18G1 rod for a 9038AG1?
Issue:
Checking on the length of a 1091S18G1 rod for a 9038AG1

Product Line:
9038S Float Switches

Environment:
Pressure, Vacuum and Float Switches

Resolution:
It is 30`` long. This is not a valid number to order though. It can be ordered as 9049 A-6, A-6A, A6-C, or A6-CS to get complete kit for float, which includes 2 of these rods. Or, if ordering additional lengths to add to one of these above kits, order as 9049T1, T1A or T1S..

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings