Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What size control power transformer is required for the 8536SEO NEMA size 3 starter?
Issue:
Transformer size for an 8536 NEMA starter

Product Line:
NEMA Type S Starters

Environment:
Square D Non-Reversing Starter

Resolution:
Standard Capacity (Form FF4T) requires 9070TF150**. TF transformers include factory installed primary & secondary fuse blocks.** Complete part number with voltage code.

Note: Standard across the line starters (8536SEG, etc) do not provide space for control power transformers and will required oversized enclosure.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings