How can we help you today?

Are the GV2 and GV3 Manual Starters DIN Rail Mountable?

Issue:
Looking if the GV2 and GV3 manual starters are DIN rail mountable

Product Line:
Operating Mechanisms and Disconnect Switches

Envinronment:
TeSys GV Manual Starters

Resolution:
Yes, they are din rail mountable.  Any 35mm DIN rail (DIN 3) is used for the GV2 and GV3 series starters.