Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the finish of QO and Homeline, NEMA 1 load center covers and boxes?
Issue:
Product Design features

Product Line:
QO Load centers

Resolution:
ALL the QO and Homeline, NEMA 1 load center covers and boxes are made of sheet steel and painted (or finished) with an ANSI 49 gray paint electrodeposited over clean phosphatized steel.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings