Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How is the mechanical interlock kit LAD9R1V installed?
Issue:
How do you install the LAD9R1V interlock kit?

Product Line:
TeSys D line contactors and accessories

Environment:
Products sold and used in the United States

Resolution:
The 2 identical TeSys contactors have removable covers on the sides at the top on either side of the contactors. These are removed and discarded. The mechanical interlock component is inserted into the slots of the right and left side contactors which are now close side by side. The supplied control bus is then connected to coils to provide electrical interlocking. Line and load side power connections are also provided.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings