Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the coil voltage codes for the LC1D40 / LC2D40 through LC1D95 / LC2D95 TeSys contactor?
Product Line:

Tesys D line Contactors

Resolution:

The following list the more common voltage suffix codes for these product lines. For a more comprehensive list and to determine compatibility with a given product, refer to the voltage code tables listed on pages 115 & 116 of the attached link.

Note: Coil Code ending number represents frequency rating as follows:
5 = 50 Hertz
6 = 60 Hertz
7 = 50/60 Hertz

AC Volts ___Code AC Volts ___Code
12 ___ J5 240 ___ U5 or U6 or U7
20 ___ Z5 or Z6 or Z7 256 ___ W5
24 ___ B5 or B6 or B7 277 ___ W6
42 ___ D5 or D7 380 ___ Q6 or Q7
48 ___ E5 or E6 or E7 400 ___ V5 or V7
100 ___ K7 415 ___ N5 or N7
110 ___ F5 or F6 or F7 440 ___ R5 or R6 or R7
115 ___ FE5 or FE7 480 ___ T6
120 ___ G6 or G7 500 ___ S5
127 ___ G5 575 ___ S6
200 ___ L7 600 ___ X6
208 ___ L6 or LE7 660 ___ Y5
220 ___ M6 or M7
230 ___ P5 or P7

Standard Coil Wide Range
DC Volts ___Code DC Volts ___Code
12 ___ JD 12 ___ JW
24 ___ BD 24 ___ BW
36 ___ CD 36 ___ CW
48 ___ ED 48 ___ EW
60 ___ ND 72 ___ SW
72 ___ SD 110 ___ FW
110 ___ FD 220 ___ MW
125 ___ GD
220 ___ MD
440 ___ RD




Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings