Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a Category B installation for Medium Voltage metal-enclosed switchgear?
Issue:
What are the Installation Categories for Medium Voltage Switchgear?

Product Line:
Medium Voltage Metal Enclosed Switchgear

Environment:
Maintenance

Cause:
Installation

Resolution:
The Enclosure Installation Category Definitions are as follows:

CATEGORY A - Provide a degree of protection against contact with enclosed equipment in Ground level installations subject to deliberate Unauthorized acts by Members of the Unsupervised General public.

CATEGORY B - Is the same as above except it's not subject to Unsupervised General public. it provides protection to Unauthorized and Untrained Personnel against incidental contact.

CATEGORY C - Is the same as A except in secured Installations accessible ONLY to Authorized Personnel.










Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings