Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a manual transfer kit accessory available for the Homeline load centers that allows the interlocking of two adjacent branch circuit breakers for a generator application?
Issue:
Product features

Product Line:
Homeline load centers

Resolution:
No, there is no manual transfer equipment kit accessory for the Homeline load centers. Consider using the QO load centers or the standard generator interlock kits for the Homeline load centers.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings