Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can be used in place of a 9013FTG**** since this comes in large carton quantities?
Issue:
Can the 9013FSG be a substitute for 9013FTG?

Product Line:
Pressure Switches

Environment:
9013FTG and 9013FSG

Resolution:
Universal replacement is the 9013 FSG2, FSG9 or FSG10.
Note: The FTG does not share all the same features nor operational characteristics as the FSG. The FTG includes the Metal flange, Form U, 2 ground screws and UL and CSA approvals.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings