Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement 220 volt direct current control coil for the LP*D12** or LP*D12**?
Issue:
Identify a replacement DC coil for an LP contactor

Product Line:
Class LP Contactors

Environment:
Schneider Electric IEC Contactors and Starters

Resolution:
For standard coil (code MD) order LX4D4MD, for wide range coil (code MW) order LX4D4MW. Note these replacement coils are for D2 Series pre-Tesys contactors only.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings