Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Customer asks if the 9001BG201 start/stop push button station is for a 3ph starter?
Issue:
Can 9001B Control stations be used to control both a single phase and a 3 phase starter?

Product Line:
Push Buttons and Operator Interface

Environment:
9001B Control Stations

Resolution:
Customer was advised that the start/stop contacts are wired into the coil circuit of the starter. It does not matter whether the starter is 3ph or 1ph. The contacts simply make and breaker the coil circuit.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings