Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the operating temperature of 8502 / 8536 devices?
Issue:
Identifying operating temperature of a NEMA contactor or starter

Product Line:
NEMA contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Identifying operating temperature of a NEMA device

Resolution:
NEMA Standard which requires 0 to 40 degrees centigrade.

This rating also applies to 8538, 8539, 8606, 8630, 8640, 8702, 8736, 8738, 8739, 8810, 8903, 8940 and 8941 devices.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings