Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the DC rating for the QMB panel?
Issue:
DC voltage rating for the QMB panels

Product Line:
QMB panelboards

Environment:
Products sold in North America

Resolution:
The QMB panels are rated up to 250VDC

NOTE: THE AIC RATING OF THE PANEL WILL BE LIMITED TO 10K.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings