Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the main breaker in a Mini Power Zone series rate w/ the downstream breakers for a higher AIR rating?
Issue:
Series Rating

Product Line:
Mini Power Zone MPZ/B
Environment:
Low Voltage Transformers

Cause:
Series Rating Main Breaker in MPZ/B Products

Resolution:

Series rating downstream of the Mini Power-Zone (MPZ) package unit substation is unnecessary. The MPZ is a UL listed device and the Transformer does not allow peak let through currents higher than the secondary type QO breakers can accommodate. The AIR of the device matches the AIR rating of the primary breaker, depending upon which catalog number is chosen.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings