Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the QO2L30S load center accept a two pole GFI, EPD, or CAFI breaker?
Issue:
Product Design Features

Product line:
QO load centers

Resolution:
The QO2L30S is a single phase, 3 wire load center with 2 pole spaces and it will accept a two pole or 2 single pole standard QO breakers. BUT it will not accept EPD, GFI, or CAFI breakers.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings