Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a CAFI and a DF breaker?

Issue:
What is the difference in a CAFI Combination Arc Fault Circuit Breaker and a DF Dual Function breaker?

Product Line:
Circuit Breakers

Resolution:
Combination arc fault circuit interrupters protect branch circuits and all downstream receptacles and cord sets against both high energy parallel arcing (the same as existing branch/feeder AFCIs) and low energy series arcing. A dual function device combines combination arc fault protection with Class A ground fault (people) protection.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings