Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are electrical interlocks available for the 9422C**** flexible cable circuit breaker operating mechanisms?
Issue:
Identify the available parts for an operating mechanism

Product Line:
9422 Operating Mechanisms

Environment:
Square D Operating Mechanisms

Resolution:
Yes, 9999R26 for single pole double throw or 9999R27 for double pole double throw.

Note: This does not apply to GJL, or Merlin Gerin (MG-NSF & MG-NSJ) flexible cable circuit breaker operating mechanism. These particular breakers require internally mounted auxiliary contacts for this purpose.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings