Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why are alternate lugs not available for safety switches as they are for molded case circuit breakers?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty, Double Throw Safety Switches and Molded Case Circuit Breakers

Resolution:
The safety switches are designed as complete devices with their own enclosures and wire bending space provided for the maximum rating of the switch. Circuit breakers are a component of a larger device (or enclosure) which may allow for multilple and/or larger conductors to be used.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings