Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When Rear Panel Mounting a VCCF3 or VCCF4, How Short Can The Shaft Be Cut?
Issue:
Minimum panel depth and shaft length for vario switches

Product Line:
Motor Disconnect Switches

Environment:
Vario Switches

Resolution:
When rear mounting the switch a shaft extension is required. The minimum enclosure depth required is 5.5". The switch itself is approximately 2.56" so the shaft extension would be 2.96" minimum length.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings