Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is included in a 9998DRC1, 9998DRC2, 9998DRC3, or 9998DRC4 contact kit?
Issue:
9998DRC1, 9998DRC2, 9998DRC3, 9998DRC4 parts

Product Line:
Definite Purpose Contactors

Environment:
Products sold and used in the United States

Cause:
Identifying Kit Contents

Resolution:
Movable contact, stationary contacts, contact spring, contact screws, binder head screws (DRC1 through 3 only), torx screws (DRC4 only), and quick connect terminals all in a polybag imprinted with quantity, Class, Type, description, bar code (if any), Square D plant code, date code, and country of origin. For the DRC4 the label is also marked ``Torque box lug screws to 35 in.-lb.``. For the DRC1 through 3 the label is also marked ``The contents of this kit are intended to service one pole.``.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings