Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What is the part number of the tie channel / Joint Cover for an AP2520G10ST length of Busway?
Issue:
What is the part number of the tie channel/ Joint cover, for an  AP2520G10ST piece of Busway?

Product Line:
I Line II Busway

Environment:
Maintenance

Resolution:
There are 2 Tie channels/Joint covers, per joint of Busway and is part number  45216-108-01 with (1) 45132-001-51 bag of 16 screws (8 used for each channel/cover), needed for installation. See video below:

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings