Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 9001 potentiometers rated for wash down applications?
Issue:
9001 Potentiometer NEMA ratings for wash-down applications

Product Line:
9001 Potentiometers

Environment:
30mm Push Buttons

Resolution:
Yes they are rated for NEMA 4 (hose directed water) and 12 applications. They are not UL listed.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings