Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the control coil voltage range and tolerance for a 8501 type X relays?
Issue:
What is the control coil voltage range and tolerance for a 8501 type X relays?

Product Line:
Relays and Timers

Environment:
8501X Control Relays

Resolution:
The tolerance on these relays depends on the type of operation:
AC operation +10 / -15%
DC operation +10 / -20%
DC dual rated +10% of larger and -20% of smaller

The control voltages are as follows:
AC Voltages
AC Voltages - HzCode
12-60V11
24-60V01
24-50V12
48-60V18
48-50V16
120-60/110-50V02
208-60V08
240-60/220-50V03
277-60V04
480-60/440-50V06
600-60/550-50V07

DC Voltages
DC Voltages for 8501XUDO Relays OnlyCodeDC Voltages for 8501XDO RelaysCode
6V506V50
12V5112V51
24V5324V53
48V5632V54
125V6348V56
250V6772V58
--90V59
--115/125V62
--230/250V66

NOTE: Some of them may not be available

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings