Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a QOU-EPD circuit breaker available?
Issue:
Is there a QOU Breaker with 30mA pick-up settings?

Product Line:
Circuit Breakers

Resolution:
There is no QOU-EPD. A QO120EPD and an OEM mounting base can be used for unit mount applications, but there is no DIN rail mountable option.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings