Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Looking for a handle electrical interlock 8539SCG44, with GJL breaker disconnect.

Issue:
Handle electrical interlock for 8539SCG44 with GJL breaker disconnect.

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Combination Starters

Cause:
Repair parts for combination starters

Resolution:
There are NO external auxiliary interlock kits available for the operating mechanism used to operate the Type GJL circuit breaker. One auxiliary contact (NO or NC) can be added to the inside of circuit breaker case. This contact module can be added at any time. Operating mechanism must be removed in order to install the contact module.
Note:

Be aware that the status of the contacts will change when when the circuit breaker trips in addition to the breaker being turned ON and OFF.
Contact Module information:
1. Catalog number is AAC
2. Form ``C`` contact arrangement



CTA-ID : 2014543

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings