Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many contact blocks can be stacked on an XB5 operator?
Issue:
XB5 contact stacks

Product Line:
Harmony XB5/ZB5 Plastic Push Buttons

Environment:
22mm Push Buttons

Resolution:
The contact blocks enable variable composition of body sub-assemblies and can be stacked to 3 rows, either: 3 rows of 3 single contacts or 1 row of 3 double contacts + 1 row of 3 single contacts (double contact blocks occupy 2 rows).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings