Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for replacement finger safe power terminal connectors for the LC1D115, LC1D150, LC1D11500 or LC1D15000?
Issue:
Identifying finger safe power terminal connector part numbers

Product Line:
Tesys D Contactors

Environment:
IEC Contactors and Starters

Cause:
Finger safe power terminal connectors required

Resolution:
For LC1D115 or LC1D150 Tesys version order LA9D115603B, this is a three pole connector and will require one kit line side and one kit for load side.

For LC1D11500 or LC1D15000 D2 Series (Pre-Tesys) version order LA9D115603, this is a three pole connector and will require one kit line side and one kit for load side.

Note: The only difference between these terminal kits is the color; the LA9D115603B is black and the LA9D115603 is beige. The parts are backward/forward compatible.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings