Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the replacement latch mechanism available for the Class 8903 Type LX mechanically held lighting contactor?
Issue:
Is the replacement latch mechanism available for the Class 8903 Type LX mechanically held lighting contactor?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Cause:
Need to replace the latch mechanism

Resolution:
Yes, order Class 8903 Type LXL*.

* Complete with proper voltage code (ex: 120 volt control; 8903LXLV02).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings